05-23-2022 02:45 PM
Hi All,
I have an XCS drive which shares it's DC bus with an XMD drive, and wish to control the power as per "2.6. Variant: Automatic load of DC bus to power ON" in the help page https://developer.community.boschrexroth.com/t5/Store-and-How-to/Suitably-Power-ON-OFF-ctrlX-DRIVE/b...
When configuring the XMD drives digtal inputs, setting an digital input to parameter DC Power Bus Control S-0-0240 and attempting to move to operating mode leads to this error: "C0242 Multiple configuration of a parameter ->S-0-0423". I believe this is because the DC Power Bus Control is also set cyclicaly by the ethercat master, however I cannot work out how to deactive this. How can I resolve this error?
Solved! Go to Solution.
05-23-2022 04:12 PM
Please provide parameter file.
05-23-2022 04:36 PM
05-24-2022 08:10 AM
The entry S-0-0240 in S-0-0024 needs to be removed in the XMD drives using the configuration possibilities for cyclic parameters within the EtherCAT control.
05-24-2022 10:24 AM
Thanks very much Drives_Uwe