10-25-2023 10:27 AM
Hi
Can you help me with specification of this motor MS2N07-C0BNA-RSVB0-NCNNN-NN, i need to put all specification manualy to Indraworks, because some parameters i can't find in datasheet (direct axis induction of motor, Quadrature axis induction of motor.....)
Thank you
Solved! Go to Solution.
10-25-2023 01:23 PM
If an MS2N motor is correctly connected to a Bosch Rexroth drive controller, no manual input of motor data is required. The data is read from the data memory in the motor during startup.
10-25-2023 01:24 PM
But on this motor is resolver which don't have this memory
10-25-2023 01:30 PM
Indrawoks & CtrlX DRIVE Engineering also have a database to look up and import respectively