cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Maximum XMD 6A from an XCD 23A

Maximum XMD 6A from an XCD 23A

bclapperton
New Contributor

I have an application for a large number of small axes (280 total). Motors are MS2N03-D0BYN. Maximum torque at standstill is 0.72Nm. Power while moving is only 100 Watts each.

The preferred combination would be Qty 8. XMD 6/6 powered by Qty 1. XCD 23/23 for a total of 18 axes.

 

 

2 REPLIES 2

Drives_Uwe
Community Moderator
Community Moderator

The combination as you want to configure would function. See attached IndraSize file. You could even go to 24 axes at 1x XCD.

Thanks Uwe. Sorry but I can't see the attached Indrasize file. Maybe I just don't know where to look.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist