F8115 is shown after update driver plus firmware

F8115 is shown after update driver plus firmware

sun_lei
Established Member

Hello  ,

       There  is a error message F8115 shown after update the driver plus(with core)  firmware to FWA-XD1-AXS-V-0308N-NN.03 ,

        but the same driver can work base the firmware  FWA-XD1-AXS-V-0306N-NN. & FWA-XD1-AXS-V-0304N-NN without error. 

       

       So is the reason about the limit of the hardware or something else ?   the information about the hardware please see attachment file.

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

This error is occurring if the firmware of the ctrlX DRIVEplus is not fitting to firmware of the integrated ctrlX CORE. See release notes for further information.

Thanks a lot for your reply~

So,if update the runtime of core first and then do the driver  firmware update (0308/0312) ,there is no error message (F8115..) shown ~

(By the way , the sequense is different  from "Guideline for the update to XCR-V-0112" ,the manual   is shown that for ctrlX DRIVEplus with integrated ctrlX CORE need to do driver firmware first .)

 

CodeShepherd
Community Moderator
Community Moderator

So it is working on your side now and this thread can be closed?

In the later version of the ctrlX CORE and ctrlX DRIVE firmware the sequences doesn't matter anymore to get everything to work.

Starting with the drive is mentioned because you can use the communication via the control to do so. Starting with the drive control will make a display necessary because this will get the only communication way. So we did not change the description for usability reasons.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist