11-17-2022 08:17 AM
Hello ,
There is a error message F8115 shown after update the driver plus(with core) firmware to FWA-XD1-AXS-V-0308N-NN.03 ,
but the same driver can work base the firmware FWA-XD1-AXS-V-0306N-NN. & FWA-XD1-AXS-V-0304N-NN without error.
So is the reason about the limit of the hardware or something else ? the information about the hardware please see attachment file.
Solved! Go to Solution.
11-17-2022 08:31 AM - edited 11-17-2022 08:31 AM
This error is occurring if the firmware of the ctrlX DRIVEplus is not fitting to firmware of the integrated ctrlX CORE. See release notes for further information.
11-18-2022 07:01 AM
Thanks a lot for your reply~
So,if update the runtime of core first and then do the driver firmware update (0308/0312) ,there is no error message (F8115..) shown ~
(By the way , the sequense is different from "Guideline for the update to XCR-V-0112" ,the manual is shown that for ctrlX DRIVEplus with integrated ctrlX CORE need to do driver firmware first .)
11-18-2022 07:37 AM
So it is working on your side now and this thread can be closed?
In the later version of the ctrlX CORE and ctrlX DRIVE firmware the sequences doesn't matter anymore to get everything to work.
Starting with the drive is mentioned because you can use the communication via the control to do so. Starting with the drive control will make a display necessary because this will get the only communication way. So we did not change the description for usability reasons.