FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
07-20-2023 03:09 PM
Is it possible to change the wifi network of the CORE? Or assign it to a different Wifi?
I can add a new network, it is then displayed in "KNOWN" under Netweork Interfaces, but the CORE does not connect to it.
Even if the previous Wifi is removed.
Is it relevant whether it is a 2.4 or 5 Ghz network?
Solved! Go to Solution.
07-20-2023 03:31 PM
What hardware are you using? The ctrlX CORE does not have a wifi adapter internal.
07-20-2023 04:03 PM
I am using a ctrlX CORE with Wifi Dongle. And its working with the current Wifi im connected to, but i need to change it.
07-26-2023 01:39 PM
In the network menu you should have a WiFi tab. There you can delete your current connection and crete a new one with the '+' button. See below
This is using version 1.20