06-26-2024 04:54 AM
There is no option for CtrlX Core X7 to upload bin file. Any one have any idea how is this possible? I try to factory reset also not possible to factory reset.
Solved! Go to Solution.
06-26-2024 07:45 AM
Did you already try to clear your cache or use a different PC? It could be that corrupted data is stored in the browser that prevents page from loading.
06-26-2024 09:41 AM
I tried another laptop that has not been connected to any ctrlX yet, result still the same.
06-26-2024 10:21 AM - edited 06-26-2024 10:36 AM
Could you check your system image version?
06-26-2024 10:27 AM
06-26-2024 10:54 AM - edited 06-27-2024 11:24 AM
As free for sales from system version 2.x on, please try reflashing the control with the latest image 2.6.1 available as early adopter version on our collaboration room.
For getting access see "FAQ for ctrlX Store".
For update see "Partition a disk as GPT & Restore ctrlX CORE X7".
06-27-2024 02:39 AM
If X7 only supports version 2. Then why we can select version 1 ctrlX PLC license in SOS?
06-27-2024 02:51 AM
If you see links below it uses 1.20.9 as requirement.
06-27-2024 11:31 AM
I adapted my post above, to be more clear.
For your problem please download the latest 1.20.13 system image (out of the 1.20.9 overall system patch) and do an image update again, to make sure file is not corrupted and imaging process was completely successful. If problem still exists please send me a private message with your contact data to have a direct look to it.