FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
06-09-2023 02:01 PM
Hi,
i like to use the numpad function by a rocker button widget. I use Step = 0.1 and Precision = 1. The rockerbutton let me step by 0.1 STeps. But if i like to input the value by the numpad a hint apperd that only integer value is accept. I item type i use is also a float number.
I like to insert with the numpad a value like 2.4! Is it possilve
Solved! Go to Solution.
06-09-2023 02:06 PM
Can you please provide a simple HMI that illustrates this issue and attach it here?
06-09-2023 02:48 PM
have a look to this picture
06-09-2023 03:07 PM - edited 06-09-2023 03:10 PM
Please see the attached HMI to see that it works without any issues.
Please rest assured that whenever I ask for an HMI that I have already thought about it and tested it. This is not a general issue, but a specific issue with your HMI, probably through some misconfiguration somewhere. It might also indicate a bug, but we need a simple HMI that illustrates this.
Please note that if you configure an item as FLOAT in WebIQ but your OPC-UA server has it as INT WebIQ will be forced to use INT automatically to be able to communicate with your OPC-UA server without syntax errors.