cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Webiq stuck in workspace related tasks cant load project anymore

Webiq stuck in workspace related tasks cant load project anymore

AndroidzZ
New Contributor

Hello,

When i wanted to publish my HMI is was stuck in publishing app. I had to alt f4 after that i tried reloading a different app, this worked. Than clearing the workspace and it got stuck in clearing workspace.. No everytime i tried to upload a project and load it is tels met that i have to unload the project first, which i cant. See image. I also tried deleting the workspace %appdata%/webiq-designer. But still after that i get the same message.

AndroidzZ_0-1674650110539.png

AndroidzZ_1-1674650118337.png

AndroidzZ_2-1674650124014.png

 

 

7 REPLIES 7

webiq-sk
Frequent Contributor

In case you are using WebIQ 2.13 please download the log file from the Runtime Manager at http://{CTRLX_IP}:10123 and attach it to this post:

webiqsk_0-1674650945204.png

If you are not using WebIQ 2.13 (please note: both your development system AND ctrlX have to use the same version 2.13 - you cannot simply update your local system without updating WebIQ on ctrlX) please update to 2.13 first, then reproduce the error, then please provide the log file.

webiq-sk
Frequent Contributor

Please also provide %APPDATA%\webiq-designer\designer.log 

I am using 2.12.1 as ctrlx runtime and 2.12.0 as designer, there is no 2.12.1 designer availible. Server app 2.13 is not availble on the collebaration room so it wont be an option to update to 2.13.

Log in the attachment

 

webiq-sk
Frequent Contributor

In the collaberation room for WebIq there is only 2.12.1 available? 

AndroidzZ_0-1674719812671.png

See the link provided above. If you cannot see it feel free to send me a private message with your contact data so we can have a look together to it:

EDIT: There is problem with our servers at the moment. We are working on it.

Collaboration room WebIQ Designer and server 2.13.0Collaboration room WebIQ Designer and server 2.13.0

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist