02-04-2022 03:01 PM
Hej,
To access variables on my ctrlX core, I am setting setting up a new entry in the IO Manager section of WebIQ Designer (ver. 2.10.0 [for the server app, too]) as follows:
I do recieve a certificate in the OPC UA Server section in ctrlX Works, but everytime I 'trust' it, another identical one pops up. Then I will have to delete the previous one to 'trust' the new one:
Still, it does not seem to help me connect to the ctrlX in Designer. It keeps statin "waiting_for_reconnect".
Any tips?
P.S. the username and password in the first picture - are those the ones used to log into the core, as well?
Solved! Go to Solution.
03-18-2022 10:05 AM
Hey,
for me the Endpoint URL is: opc.tcp://ctrlx-CORE:4840
Loggin in with the default user and password works for me but for security reasons, I created an idividual user, which is only able to access the datalayer and opcua server.
cheers