Web IQ server and Ubuntu Core20

Web IQ server and Ubuntu Core20

ILS
New Poster

I was trying to install the WebIQ server runtime app V2.10 on the ctrlX Core with RM 21.07 but I got an error message saying that this is not compatible with ubuntu Core20.

Will there soon be a new version of the WebIQ server which will be compatible?

 

3 REPLIES 3

bschmidt
New Contributor

I've run into this also. I've had to install core18 to RM21.11 to support WebIQ. So core18 and core20 are running on the same device. 

Zimmbo
Established Member

Hi all,

dear WebIQ Team, please let us know, if an update for WEBIQ Server app is available or will be available.

If the ctrlX Core is updated to the Core20 system the HMI not working anymore.

Hello

  • The WebIQ team is working on an update. Currently no finishing date available.
  • Workaround to use the WebIQ app V2.10 with the RM21.11: Install core18 paralell to core20. (like mentioned in the thread before)
  • Possible problems at drive integraded CORE if many apps (WebIQ + 3Dviewer + IDE + ...) are running. Here a solution will come with the next patch end of january 2021.

Regards

Jochen

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist