FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
06-09-2023 11:55 PM
I am seeing an issue with variables not being retained reliably in ctrlX CORE memory on power cycle. This has only become an issue after upgrading the WebIQ runtime to version 2.14.1. They were retained properly using version 2.12.
I am writing to the variables using an iq-input-field widget. Before power cycling, the variables seem to be written and read properly.
Solved! Go to Solution.
06-12-2023 08:18 AM - last edited on 06-13-2023 08:47 AM by HmiGuide
06-12-2023 03:54 PM
These are variables defined in the Process Data Manager using the internal IO handler. The persistent box is checked on these variables. No other IO handler is defined and no OPC UA server was necessary for this to work prior to updating WebIQ to version 2.14.1 and ctrlX CORE firmware 1.20. These updates were done at the same time.
I've attached the project where I am experiencing the issue. The variables are modified on the 6th view of the main screen using iq-input-field widgets.
06-13-2023 09:07 AM
I was able to reproduce this with a very simple HMI (your HMI is not in a valid format btw). I can confirm that with WebIQ from 2.14.0 on the persistence of internal items is broken. We are looking into this now.
06-22-2023 08:51 AM
This will be fixed with WebIQ 2.14.3 which will be released soon from Smart HMI.