FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
06-16-2022 08:23 AM
Hello,
When we style a radial gauge with a linear gradient we are not able to see it in the web server once it is published,
We can see it in the Designer as the image shows:
However in the web server:
The gauge is configured in this way:
When we configured the gauge with a Solid Color we did not have any problem so we assume that it is because of this type of styling,
Why is this happening? Any ideas?
Thanks in advance,
Solved! Go to Solution.
06-20-2022 07:06 AM
This is an issue that's been fixed for the new release WebIQ 2.12 which is planned to be released within the next weeks from WebIQ side. As a workaround you can just use a plain color instead of a gradient for the time being.