cancel
Showing results for 
Search instead for 
Did you mean: 

LImit the number of client connection in WebIQ

LImit the number of client connection in WebIQ

Rathinavel
Established Member

Hello,

Right now, where can i find the feature to limit the number of clients to be connected in WebIq. 2 clients are allowed by default in the exisitng version of WebIq 2.14.3.

5 REPLIES 5

webiq-sk
Frequent Contributor

You posted in the wrong forum - can an admin please move this to the correct forum?

Regarding the question: the number of clients is a license feature, i.e. if you want to add more clients you have to purchase the corresponding client pack licenses. Otherwise, no more than 2 concurrent clients are allowed to connect to your HMI.

 

Moved to corresponding sub forum "Smart HMI - WebIQ Designer and Server".

The question is can the number of clients be limited to just one?

HmiGuide
Community Moderator
Community Moderator

The question is not clear. To avoid problems with parallel session, the customer want to limit the sessions to a single session.
Therefore the question is: Can I limit the number of sessions for a specific project to 1, even if there are more clients available in the license.

webiq-sk
Frequent Contributor

There is no functionality allowing configuration of the maximum number of connected clients. It is only a license feature and cannot be restricted further.

HmiGuide
Community Moderator
Community Moderator

You can at least output the number of connected clients into a WebIQ item. It works like this:
- Create a variable in the Process Data Manager
- Select the usercount function in the simulation section

HmiGuide_0-1699344656598.png

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist