08-23-2024 01:16 PM - last edited on 10-23-2024 09:26 AM by HmiGuide
Hello everyone, I apologize in advance since I am not a web developer and I am struggling with this.
I want to use the Open Bridge web components, I tried the ones already provided by SmartHMI but I want to use the new ones from Open Bridge 5.0 . I followed the instructions on the Open Bridge github but when applying that to WebIQ it gives me errors with the Import
Uncaught SyntaxError: Cannot use import statement outside a module
How am I supposed to use this kind of web components in WebIQ? Is it just not possible or do I have to manually adapt the components as it is shown in the "lib-openbridge" and other examples given by SmartHMI?
Thank you for your help.
08-23-2024 01:44 PM
This explains the error and possible solution: https://stackoverflow.com/a/78176180
If I were you I'd check if there is a non-module version of OpenBridge and use that - the one we used is not a module: https://demo.smart-hmi.com/openbridge/js/custom-libs/openbridge.js
08-26-2024 10:52 AM
How can I add the type="module" to a local script?
08-26-2024 11:21 AM - edited 08-26-2024 11:21 AM
If I were you I'd check if there is a non-module version of OpenBridge and use that - the one we used is not a module: https://demo.smart-hmi.com/openbridge/js/custom-libs/openbridge.js
Did you check that such a version does *not* exist? If it is, it's very easy.
Otherwise it's currently more complicated.
09-05-2024 03:23 PM
You can transform the original module based javascript to plain javascript using a bundler.
For instance using rollup and rollup.config.js
export default {
input: 'src/main.js',
output: {
file: 'dist/bundle.js',
format: 'iife'
}
};
The resulting bundle.js will be a vanilla javascript file without any external dependencies.