cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Failed with result 'signal'

Failed with result 'signal'

always
New Poster

I'm trying to communicate with a basler camera through their pylon driver over ethernet.

To test if core can discover the camera, I simply just need it to print the device number of the camera,

always_0-1692337287412.png

but in the log I get the following problem

always_1-1692337333115.png

 

I am at a loss here and would appreciate some help.

5 REPLIES 5

CodeShepherd
Community Moderator
Community Moderator

Moved to corresponding sub forum SDK.

To sum things up: you pack your code into a snap install it on a ctrlX CORE and then you get the error on your picture in the logbook.

Could you add a system report of your ctrlX CORE so we get some more insights. (1.20 See in online documentation, 1.12 see documentation here)

Could you add some information about hardware topology and network settings in your application? Just to check if camera can even be reached via the network.

Does your snap have the necessary system plugs to access the network (See snapcraft.yaml)?

 snap have the necessary system plugs to access the network

always_1-1692342625343.png

I'm embarrassed that my download failed.

always_0-1692342447566.png

I just set the ip address of the webcam to 192.168.1.11 on the same network segment as core (192.168.1.1)

CodeShepherd
Community Moderator
Community Moderator

So XF10 is connected to a switch and also camera is connected to the same?

It seems you are working with system version 1.12. Can you confirm?

Which version of the SDK is used?

always_1-1692690569131.png

 


After some modifications, I am having the problem as shown in the picture above

I can determine that the core and basler cameras can communicate with each other, for example to get the device model, but I can't put the image data into ptrGrabResult
“RetrieveResult(5000, ptrGrabResult,TimeoutHandling_ThrowException)”

ptrGrabResult is the variable used to store the image capture result, it is a pointer to the CGrabResultPtr class.

Hello @always  did you solve this proble already right? expanding the MTU of the interface?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist