04-05-2023 03:29 PM
Hi,
I am using cedalo MQTT Broker on ctrlX CORE. The MQTT broker just worked for 2 days and today it promted message "License for Mosquitto Management Center required" when I opened the broker app. This message appeared after I restarted the ctrlX CORE.
Please check the error message and license screenshots.
Solved! Go to Solution.
04-06-2023 07:21 AM
Hello Akseer
what version do you use
Do you have other functional apps installed (like Motion, PLC, OPC-UA,...). If yes is their license problem too.
Maybe first you can check the time settings. In older versions there was a problem with the license manager and a wrong time.
Regards
Jochen
04-06-2023 01:52 PM
04-10-2023 07:40 PM
Hello Akseer
So the problem vanished suddently after ctrlX CORE restart.
Let's see if the problem occure again.
Regrads
Jochen
04-11-2023 10:56 AM
Hi Jochen,
The issue persists. The Cedalo MQTT Broker "Management Center" either works as usual or randomly shows the two error messages as shown in figures below.
The time on ctrlX device is also synchronized with a NTP server, so time does not seem to cause the issue. Please have a look at the picture below.
Please let me know about the possible troubleshooting measures. Thanks
04-17-2023 08:41 PM
Hi,
The issue is now resolved after updating the Mosquitto MQTT Broker app.
Thanks
08-17-2023 03:26 PM
Hello.
I seem to have the same problem on my 2 cores.
I attached picture of all apps so all the versions can be seen there. Is there newer version of the MQTT broker?
Also time on core is set correctly.
How could I solve this?
09-04-2023 11:04 AM
Hello,
Any update on this issue? I have a similar problem and How to solve it?
The Cedalo Mosquitto version I can find and install is 2.0.16.
Regards
09-05-2023 07:01 AM
Hi @Lauri , Hi @chockalingam ,
Cedalo updated their Mosquitto app. It is currently in validation.
Please contact me via message here for a quick solution.
Regards,
Michael