04-15-2024 02:16 PM
Hello,
Is it possible to write to MLD array variables? I can see for example ReadVariableBySymbolArrayInt but not a Write equilvalent?
If it is possible is there a maximum number of array elements you can write to using eal4DotNet?
Many thanks
Solved! Go to Solution.
04-18-2024 10:15 AM
Hello.
That works (MLD IndraDrive), you can test it with the "drivetool.exe", see screenshot.
04-22-2024 03:45 PM
Thanks. I found by testing that it worked using "WriteVariableBySymbol" so this caters for multiple data types and the size limit appears to be 1400 bytes.