07-10-2024 10:07 PM
Hey there. Working on a project to test an energy harvesting system. I want to automate the testing procedure of the system and for that I want to create various motion profiles/control loops/cycles with changing parameters (velocity, position, torque, etc), with diferent durations. I want to know if I can create those types of motions/loops using the IndraWorks Ds software. And if so how? Can I define motion profiles directly in IndraWorks Ds and automate those motion sequences using function blocks and control buttons? My goal is to automate the testing procedure as much as possible (aka click in as few buttons as possible (just in the beginning, then system shall be autonomous)).
Would appreciate if someone could help. Thanks
07-11-2024 09:56 AM
There are two possible ways:
We will come with some more detailed information in the next days.
07-11-2024 04:30 PM
Thanks a lot. I will investigate further and wait for the more detailed information you may provide me.
08-20-2024 04:22 PM
Hey there @CodeShepherd. Do you have more detailed information? Would be glad if you could help futher. Thanks.
09-04-2024 09:46 AM
Sorry for the late reply.
You can use the online help included in IndraWorks DS or download the functional description of IndraDrive MPx-20 Functions.
See chapter "8.7.4 Sequential Block Processing" or also "10.3 Rexroth IndraMotion MLD (Drive-Integrated PLC)"
09-04-2024 01:14 PM
Thanks a lot for the reply. Can I reach my goal using the software IndraWorks Ds or do I need the software IndraWorks Engineering (with license)?
09-05-2024 11:17 AM
For case one Indraworks DS is fine, for case two Indraworks MLD will be needed.
09-05-2024 05:51 PM
Ok, thanks. So my endgoal is this:
I want to automate the testing procedure of an energy harvesting system and for that I want to create various motion profiles/control loops/cycles with changing parameters (velocity, position, torque, etc), with diferent durations. My goal is to automate the testing procedure as much as possible (aka click in as few buttons as possible (just in the beginning, then system shall be autonomous)).
How can I reach my goal more effectively: using case one or case two?
I assume case one to be:
and case two to be:
How then can I reach my goal more efficiently, effectively and easily? Should I opt for case one or case two?
09-06-2024 08:28 AM
As your premises are more on light wait programming and easy handling I would recommend case one.
If you need different motion profiles you could simply create them once in the IndraWorks DS and then export the needed parameter (for quicker loading not use all but create a fitting parameter group) so they can easily be loaded again to the drive.
09-06-2024 06:12 PM
Ok, thanks a lot. So I can use IndraWorks Ds. I am a beginner to all this. Do you have any resources where I can learn how to do what you suggested or could you give me some lights and help on how to do it using IndraWorks Ds? I would be extremely thankful.
Thanks you very much once again.
09-09-2024 08:35 AM
I am not quite sure what you expect. Please first have a look to the manual mentioned above.
A general good entry point is our how to collection in this ctrlX AUTOMATION Community. There you can find all kind of helpful information.
10-02-2024 02:36 PM - edited 10-02-2024 02:36 PM
Thanks a lot for the reply.
This is my endgoal:
I want to automate the testing procedure of an energy harvesting system and for that I want to create various motion profiles/control loops/cycles with changing parameters (velocity, position, torque, etc), with diferent durations. My goal is to automate the testing procedure as much as possible (aka click in as few buttons as possible (just in the beginning, then system shall be autonomous)).
To achieve this goal I want to use the IndraWorks Ds software.
Can you help me? Could we arrange a quick call so that I can explain you everything in more detail in order for you to help me?
Would be extremely thankful.
2 weeks ago
As we cannot see contact data for data security reasons, please send me a private message with your data to get in contact.