cancel
Showing results for 
Search instead for 
Did you mean: 

Indraworks Version

Indraworks Version

Kenyo
New Poster

Hi,

I'm trying to install Indraworks ML 14V22 P12 and Indraworks ML 15V18 on the same laptop because I need to open both versions because we have many machines with 14V and 15V. Everytime I install one version it overlap the other and I cannot open them at the same time.

 

6 REPLIES 6

Sgilk
Contributor

@Kenyo ,

One suggestion would be to install each version in a seperate virtual machine. Someone may well have a tip to have both versions on a host system though.

ctrlXProgrammatore
Long-established Member

Hello @Kenyo 

Depending on which version you are installing second a selection can be made during the installation that will install it instead of updating the previous installed version.

For IW 14 select Extended then New Installation:

ctrlXProgrammatore_0-1724245630808.png

ctrlXProgrammatore_1-1724245654581.png

I also like to change the installation name so it matches the installation version, for example:

ctrlXProgrammatore_2-1724245707028.png

If IW 15 is being installed second, select Reinstall:

ctrlXProgrammatore_3-1724245788737.png

 

HTH

 

 

 

Hi!

I tried it but now when I try to open the version 14 i get this window.

Kenyo_0-1724853197566.png

 

ctrlXProgrammatore
Long-established Member

Hello @Kenyo ,

Does IW15 open without any problems? 

Do you have administrator rights on the PC? If so, can you try right clicking on the IW Engineering icon then select "Run as adiminstrator":

ctrlXProgrammatore_0-1724854538555.png

 

 

PS: Regarding your statement at the top: "... and I cannot open them at the same time". 

That's not possible in the same OS. Means, when V14 is running you can't run V15 as well and vice versa. To do this, you need to run the V14 and V15 in different OS; eg. using virtual machines. 

Thoomas
Community Moderator
Community Moderator

Any new remarks, progress, issue solved ...? 

Otherwise we will close it due to inactivity ...

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist