03-05-2024 01:58 PM
03-08-2024 11:56 AM
The error itself is telling that a parameter was added to the cyclic data that is not allowed to be.
Was was done before the error occurred the first time? Have there been any changes in firmware version, parameter settings or or any Startup parameters added?
Please beware that the EtherCat master on switching up the fieldbus is writing several parameter of drives like e.g. the address.
03-08-2024 12:05 PM
Please provide parameter file in the faulty state in format "all parameters". As "CodeSheperd" tells something is wrong in the assigning of the real time data.
09-05-2024 11:04 AM
Are there any news? Can this topic be closed?