FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
02-14-2024 04:28 AM
Hello,
Is there a device description file or setting that will populate the list when you are adding process data to an IndraDrive in I/O Engineering? For ctrlX DRIVE a selection list would show here. For IndraDrive you have to type the parameters manually.
Best regards,
Brian
Solved! Go to Solution.
03-13-2024 08:15 AM - edited 03-13-2024 08:16 AM
Moved to corresponding sub forum IndraWorks, IndraControl for MLC/MTX, IndraDrive.
Sorry for the late reply. This lists are not available for IndraDrives. You have to enter them manually.
03-19-2024 02:33 PM
I had just the same issue. While adding the parameters (IndraDirve) manually it is very useful to give the parameters a name to find it easily in the DataLayer and/or PLC !!!
Then the parameter are easy to assignable in the PLC:
and of course to find in the DataLayer:
09-11-2024 08:57 AM