cancel
Showing results for 
Search instead for 
Did you mean: 

Trouble Connecting WebIQ and CtrlX CORE Virtual

Trouble Connecting WebIQ and CtrlX CORE Virtual

Lide
Established Member

Hi everyone,

I'm running into a bit of trouble establishing a connection between WebIQ and CtrlX CORE Virtual. I've set the CtrlX CORE Virtual "Extended" settings to "Port forwarding", but I'm still unable to get it working.

Any help would be greatly appreciated. Thanks in advance!

6 REPLIES 6

CodeShepherd
Community Moderator
Community Moderator

Moved to corresponding sub forum "Communication".

Did you already trust the certificate via "Settings -> Certificates & Keys -> OPC UA Server"? As the client will sent his to the master and it needs to be trusted there.

Did you try using IP 127.0.0.1 instead of name of the control?

Lide
Established Member

Where do I find "Certificates & Keys -> OPC UA Server"?

CodeShepherd
Community Moderator
Community Moderator

Like mentioned certificate have to be trusted on master side. It can be done via the ctrlX OS web UI:

ctrlX OS web UI - Settings - Certificates and Keys - OPC UA ServerctrlX OS web UI - Settings - Certificates and Keys - OPC UA Server

Lide
Established Member

I have already trusted the certificate but I'm still unable to get it working.

Sgilk
Frequent Contributor

@Lide ,

Try specifying the ip address rather than the VirtualCore-2 in the WebIQ OPC UA client. Can you reach the OPC UA server from another client?

NoRisk4Project
Long-established Member

Hello,

On the first view, I miss the user authentification inside your OPC UA configuration. Did you delete this setting for the screenshot or wasn't it set at all.

2024-10-14_11h14_21.png


The OPC UA server requests a authentification via user/password, without authentification a connection is not possible.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist