FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Tuesday
Hi everyone,
I'm running into a bit of trouble establishing a connection between WebIQ and CtrlX CORE Virtual. I've set the CtrlX CORE Virtual "Extended" settings to "Port forwarding", but I'm still unable to get it working.
Any help would be greatly appreciated. Thanks in advance!
Tuesday
Moved to corresponding sub forum "Communication".
Did you already trust the certificate via "Settings -> Certificates & Keys -> OPC UA Server"? As the client will sent his to the master and it needs to be trusted there.
Did you try using IP 127.0.0.1 instead of name of the control?
Tuesday
Tuesday
Like mentioned certificate have to be trusted on master side. It can be done via the ctrlX OS web UI:
Tuesday
Tuesday
@Lide ,
Try specifying the ip address rather than the VirtualCore-2 in the WebIQ OPC UA client. Can you reach the OPC UA server from another client?