FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
09-17-2024 11:05 AM
Hi everyone,
I'm running into a bit of trouble establishing a connection between WebIQ and CtrlX CORE Virtual. I've set the CtrlX CORE Virtual "Extended" settings to "Port forwarding", but I'm still unable to get it working.
Any help would be greatly appreciated. Thanks in advance!
09-17-2024 11:16 AM
Moved to corresponding sub forum "Communication".
Did you already trust the certificate via "Settings -> Certificates & Keys -> OPC UA Server"? As the client will sent his to the master and it needs to be trusted there.
Did you try using IP 127.0.0.1 instead of name of the control?
09-17-2024 11:26 AM
09-17-2024 11:32 AM
Like mentioned certificate have to be trusted on master side. It can be done via the ctrlX OS web UI:
09-17-2024 11:46 AM
09-17-2024 04:24 PM
@Lide ,
Try specifying the ip address rather than the VirtualCore-2 in the WebIQ OPC UA client. Can you reach the OPC UA server from another client?
a month ago
Hello,
On the first view, I miss the user authentification inside your OPC UA configuration. Did you delete this setting for the screenshot or wasn't it set at all.
The OPC UA server requests a authentification via user/password, without authentification a connection is not possible.