Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Remote PLC Connection With VPN

Remote PLC Connection With VPN

aFouraker
Occasional Contributor

I am using a VPN to program/maintain a remote PLC program. This is working for going online. However, when I am online I am intermittently kicked off the remote device. Is there a parameter to allow for a longer communication timeout when connected with the PLC? 

7 REPLIES 7

Jochen_Mueller
Community Moderator
Community Moderator

Interesting issue. Haven't tried this before.

Queston:

  • Do you do the access via the DevicePortal?
  • Or do you make the VPN connection manual via the VPN app?

Maybe a saved configuration will be helpful...

aFouraker
Occasional Contributor

Direct connection with the VPN. 

Hi aFouraker,

just tested it with version 1.12 via a vpn connection europe <-> australia and back.

Ping from my engineering pc to the control was arround 515ms.

Worked fine as you can see in the video screenshot, video was not possible to upload.

Is it maybe another issue, maybe the vpn connection is interrupted, did you check the logbook?

TheCodeCaptain_0-1640107476792.png

 

Hello everyone,

Have you tried to use the VPN client functionality and the CtrlX DRIVE Engineering as well? I've been using the VPN feature with no problem to access the CtrlX-Core, but when I use the CtrlX DRIVE Engineering I can not discover the Drive.

Should I configure something on my windows Wi-Fi network (for the IPv4) ?

Any hint would be greatly appreciated. 🙂

Hi GustavoTaffarello,

there are some things you have to think of.

1. Activate EoE for the Drives and the EtherCAT Master (Pic1)
2. Enable IP forwarding for the Interfaces (Pic2)
3. Tell your PC with a route how the EtherCAT network (172.31.0.0) can be reached (Can be done automatically, by clicking the icon on the webpage, or manually with the command line) Pic 3 and 4

TheCodeCaptain_0-1683204643703.png

 

TheCodeCaptain_1-1683204700501.png

 

TheCodeCaptain_2-1683204754243.png

TheCodeCaptain_3-1683204824553.png

 

Max1
Long-established Member

Hello CodeCaptain

In china I uesd remote control box(OrayBoxR300A) like VPN,but I can't connect ctrlx core ,even though i have Enable IP forwarding for the Interfaces.

I used ctrlx works 1.14. I want to know what should i need to setting?

 

 

PREVIEW
 
 
 

Hello Max, 

Ok the VPN is installed on the OrayBoxR300A? or it provides just the internet connection?

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist