Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

CtrlX connection issue.

CtrlX connection issue.

Open
Occasional Contributor

Hello Community,

Below is my CtrlX setup.

Open_0-1658977368931.png

 

When i connect the above setup my engineering PC could not connect to 192.168.1.1

Open_2-1658976552889.png

but however it is able to read 192.168.1.1 in CtrlX work and it is able to open the CtrlX page via [fe80::260:34ff:fe8a:268e]

Open_3-1658976612980.png

Open_4-1658976655158.png

In my android tablet i am able to connect to 192.168.1.244

20220728_105458.jpg

Anyone have the same issue?

 

 

3 REPLIES 3

CodeShepherd
Community Moderator
Community Moderator

Is the setting of the network port of your engineering PC also in the correct subnet? (192.168.1.xxx)

The visibility in ctrlX WORKS is done via an IPv6 mechanism and not IPv4 that's why you can see it and connect via the IPv6.

Open
Occasional Contributor

Hello CodeShepherd,

I am trying to connect engineering PC and Android tablet is it possible to connect them to CtrlX simultaneously with internet and network cable?

My network port in my PC is connected to the correct network subnet. 

Open_0-1659314795016.png

But however when i removed the network cable connected to the internet i am able to connect through 192.168.1.1 via engineering PC.

Warmest regards,

Open

Open
Occasional Contributor

I have resolved it by changing my CtrlX engineering port IP address to 192.168.2.1. Now i am able to connect both Engineering PC and android tablet simultaneously. 

Thank you!

Warmest regards,

Open

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist