FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
07-28-2022 05:01 AM - last edited on 07-28-2022 12:03 PM by CodeShepherd
Hello Community,
Below is my CtrlX setup.
When i connect the above setup my engineering PC could not connect to 192.168.1.1
but however it is able to read 192.168.1.1 in CtrlX work and it is able to open the CtrlX page via [fe80::260:34ff:fe8a:268e]
In my android tablet i am able to connect to 192.168.1.244
Anyone have the same issue?
Solved! Go to Solution.
07-28-2022 12:06 PM - edited 07-28-2022 12:07 PM
Is the setting of the network port of your engineering PC also in the correct subnet? (192.168.1.xxx)
The visibility in ctrlX WORKS is done via an IPv6 mechanism and not IPv4 that's why you can see it and connect via the IPv6.
08-01-2022 02:49 AM
Hello CodeShepherd,
I am trying to connect engineering PC and Android tablet is it possible to connect them to CtrlX simultaneously with internet and network cable?
My network port in my PC is connected to the correct network subnet.
But however when i removed the network cable connected to the internet i am able to connect through 192.168.1.1 via engineering PC.
Warmest regards,
Open
08-01-2022 04:11 AM
I have resolved it by changing my CtrlX engineering port IP address to 192.168.2.1. Now i am able to connect both Engineering PC and android tablet simultaneously.
Thank you!
Warmest regards,
Open