Connecting physical ctrlX core to the internet

Connecting physical ctrlX core to the internet

foldenjared
Member

I am unable to connect my ctrlX core the internet. I am trying to set up an internet connection because I get an error while trying to install InfluxDB, since it is trying to retrieve core22, but it cannot due to the lack of an internet connection.

influxdb_error.png

My setup is as follows:

  • My ctrlX core is connected to my PC via ethernet.
  • My PC is connected to my home internet network.
  • I am not behind a proxy server.
  • I have configured my IPv4 ethernet connection to use a static IP address.
    • foldenjared_1-1724712390174.png

       

    • foldenjared_0-1724712313340.png

       

    • Note: I am unable to access the ctrlX via web interface in my browser at https://192.168.1.1. I am only able to access it via IPv6 connection through the Network section of my File Explorer. I'm not sure if this is relevant to the issue I'm having or not.

I am trying to connect by following the instructions in this how-to article: Connect real ctrlX CORE via proxy to the Internet (boschrexroth.com)

I have download px.exe and configured the inbound exception as described in the article. In the px.ini file, I have configured gateway = 1. This is what the program looks like when it is running. 

foldenjared_2-1724712563798.png

I have also configured the proxy settings on the ctrlX interface as follows.

foldenjared_3-1724712611378.png

The error message I recieve when trying to install InfluxDB using these settings is the one at the top of this post.

Any help would be greatly appreciated!

2 REPLIES 2

foldenjared
Member

I solved this issue. Firstly, it was important that my IPv4 connection was not working, and I fixed it by disabling my PC's WiFi adapter to eliminate any other devices on the network competing for the 192.168.1.1 address. Additionally, the proxy settings of my ctrlX core, I was listing the IP address of my ctrlX core's network adapter (192.168.1.1) when I should have been listing the IP address of my PC's network adapter (192.168.1.10).

CodeShepherd
Community Moderator
Community Moderator

You could also check our how two collection, where some articles are available for connecting ctrlX COREs to the internet.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist