cancel
Showing results for 
Search instead for 
Did you mean: 

ctrlX CORE X3 with CoDeSys ProfiNET connceting to HMC.

ctrlX CORE X3 with CoDeSys ProfiNET connceting to HMC.

CvM
Member

I want to connect a HMC with FWA-HYDRV*-HDM-20V18-D5-1-SRV-ML to my X3 ctrlX CORE. ( VRS 1.20.0
U made use of the document "Installation guide: CoDeSys Ethernet I/P and PROFINET for ctrlX CORE".

Then I added the file "GSDML-V2.4-Bosch_Rexroth_AG-011F-HydraulicDrive_03V00-20210608.xml"to my CORE and when I scan for a device I find my HMC but I get nessqages Attention: The device was not..." see printout.

CvM_1-1713358147105.png

CvM_0-1713358107027.png

When I coppied the device to my project I get the nest view!
And I it is not possible to get the conmmunication running.

CvM_2-1713358382315.png

What do I have to do to get it the communication running?

7 REPLIES 7

CodeShepherd
Community Moderator
Community Moderator

Moved to corresponding sub forum CODESYS - PLC Add-ons.

FranzClt
Established Member

have you tryed it with a other ProfiNet device

 

I didn't have time jet:(, have other things to do.
Probably in one of the comming weeks.
I will try it, and keep you informed.

CodeShepherd
Community Moderator
Community Moderator

Is this still an issue? Have there been a solution? And can this topic be closed?

Hello,
As told I was occupied with other activities.
But last week and this week I had some time to figure out one and other!

When I used the CoDeSys ProfiNet controller wit a ctrlsX Drive it worked in no mater of time:)

But when I used the HMC in combination with the proposed GSDML files it didn't work!

So what I did I tried some other combinations of firmware in the HMC and GDSML files.

And now i got my system working!

In my HMC I use firmware "FWA-HYDRV*-20V24.30-D5-1-SRV-ML".

The GDSML file that I use now is "GSDML-V2.25-Bosch Rexroth AG-011F-HydraulicDrive_01V01-20180907.xml"!

And now I have data excange.

When is use the proposed file "GSDML-V2.4-Bosch_Rexroth_AG-011F-HydraulicDrive_03V00-20210608.xml" the system gives me some errors and when I add the HMC to my project I can't delete the HMC from my project anymore.

The only way to get out was close my project without saving and re-open the old project again!

I'm writing a document with my exepriences and will add this to this item later on.

At last herby my tests results and the problems I had.

Hopefully someone else can use this information aswell.

 

CodeWasi
Occasional Contributor

Thank you CvM for your investigation.
Checked it and confirm your observes.
Do you mind to avoid the scan-based import to the project by operting with the offline adding in the meantime. 
Return with futher results as soon as I get feedback from RuD.

Thanks!

CodeWasi_0-1729667738831.png

 


 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist