04-28-2023 12:07 AM
Hi,
I'm trying to setup a web visualization and when downloading to the controller I get the error message :
[FATAL ERROR] Unresolved reference: 'CODEMGETCONTENTBYFIRMCODE2'
I'm using a virtual controller with an image of V1.12.19 and ctrlX WORKS V1.12.10. I tried with a brand new project with only an empty visualization and get the exact same error.
I read on a This thread that it might be because I have different version of the PLC app on the controller and the PLC engineering. The problem is I'm the opposit situation compared to the post. I have V1.12.5 on the controller and V1.12.3 on PLC engineering. Is there a way to
a) Update the version in PLC engineering to V1.12.5 or
b) Download the V1.12.3 of the app to downgrade it on the controller?
Thanks,
kovaley
Solved! Go to Solution.
04-28-2023 07:56 AM - edited 04-28-2023 08:01 AM
As I suggest you are trying to use a CodeSys WebVisu moved your topic to the according forum.
You will need to use at least a version 1.18 of PLC engineering. See this topic for further information. I would suggest to use actual version 1.20.
04-28-2023 01:37 PM
I can only get up to 1.12.10 for ctrlX WORK on the collaboration room. Am I doing something wrong? Anyway, thanks for your previous answer!
04-28-2023 02:46 PM
The newer versions are in pre-release state. So you need to ask for access for this software. Please have a look in the FAQ for ctrlX Store access level 3 for further information.