Hello Community,
Is it possible to upload PLC webvisu project into CtrlX core virtual and open webvisu in CtrlX virtual?
I get an error when downloading to my CtrlX virtual.
Warmest regards,
Open
Solved! Go to Solution.
The error tells you that there are firmware functions missing on the ctrlX CORE. So probably you are using a feature, that is not implemented yet. Which version of the PLC app and ctrlX WORKS are you using?
See this thread for information about the alarm handling.
Please have a look to this thread for information what is needed to use the WebVisu.
Hello CodeShepherd,
I am using CtrlX works version: 1.14.1
Warmest regards,
Open
The CODESYS Web Visu is a partner app which requires a license. The licensing mechanism for CODESYS Add-Ons is not avilable on the virtual ctrlX CORE. Most likely this is the reason for the compiler error messages. Can you compile your program if you change the device to a real ctrlX CORE?
Hello PLC2030,
Changing to real CtrlX core works.
Thank you.
Warmest regards,
Open