cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

Unexpected Building PLC Code Error

Unexpected Building PLC Code Error

ericvergara
Occasional Contributor

Hello,

Does anyone know what type of error is this?

ericvergara_0-1664287748160.png

We are using a ctrlX Core Virtual and the Softmotion and Codesys WebVisu packages but we do not have any idea why this error appears when we build the code,

Many thanks,

6 REPLIES 6

CodeShepherd
Community Moderator
Community Moderator

What did you do before the error came up first?

ericvergara
Occasional Contributor

Hello CodeSheperd,

We do not really know, as this code is programmed by a customer,

 

So as it also hard to say what causes that error, I would suggest to do a "Build -> Clean all" inside the ctrlX PLC Engineering to get rid of possible corrupted artifacts and recompile the project, if not even already tried this.

ericvergara
Occasional Contributor

Hello,

He created another PLC project and exported the logic and this error is now gone,

However, it seems that it has some problems regarding the "IoDrvEthernetIP" library, that is automatically added whent the codesys package is installed,

I attach here the pictures

 

ericvergara_0-1664461152504.png

ericvergara_1-1664461161788.png

ericvergara_2-1664461182164.png

 

This CIP Object Library inside the Ethernet/IP Library seems to have a logical error or so,

Any idea?

Thanks for the help,

 

georkueh
Community Moderator
Community Moderator

Hello, you will not succeed to run the CoDeSys Add Ons like Eternet IP Scanner/Adapter, Softmotion or Web Visu on ctrlX CORE virtual. These Add Ons require licensing components, that are currently not available with the target.

So to run these Add Ons you need a real ctrlX CORE hardware.

kind regards

PLC2030
Long-established Member

ctrlX CORE virtual will support the licensing of CODESYS Add-Ons from ctrlX Store in version 01V18.

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist