09-27-2022 04:11 PM
Hello,
Does anyone know what type of error is this?
We are using a ctrlX Core Virtual and the Softmotion and Codesys WebVisu packages but we do not have any idea why this error appears when we build the code,
Many thanks,
Solved! Go to Solution.
09-28-2022 07:26 AM
What did you do before the error came up first?
09-28-2022 08:21 AM - edited 09-28-2022 12:19 PM
Hello CodeSheperd,
We do not really know, as this code is programmed by a customer,
09-28-2022 09:18 AM
So as it also hard to say what causes that error, I would suggest to do a "Build -> Clean all" inside the ctrlX PLC Engineering to get rid of possible corrupted artifacts and recompile the project, if not even already tried this.
09-29-2022 04:21 PM
Hello,
He created another PLC project and exported the logic and this error is now gone,
However, it seems that it has some problems regarding the "IoDrvEthernetIP" library, that is automatically added whent the codesys package is installed,
I attach here the pictures
This CIP Object Library inside the Ethernet/IP Library seems to have a logical error or so,
Any idea?
Thanks for the help,
10-13-2022 11:36 AM
Hello, you will not succeed to run the CoDeSys Add Ons like Eternet IP Scanner/Adapter, Softmotion or Web Visu on ctrlX CORE virtual. These Add Ons require licensing components, that are currently not available with the target.
So to run these Add Ons you need a real ctrlX CORE hardware.
kind regards
11-17-2022 10:18 AM
ctrlX CORE virtual will support the licensing of CODESYS Add-Ons from ctrlX Store in version 01V18.