FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
09-23-2022 10:20 AM
Hello everyone,
I found in the CodeSys Store the following from BE.Services
This product allows the configuration of POWERLINK networks.
Industrial Control Systems implementing CODESYS can easily be turned into a POWERLINK Master (Managing Node – MN). The integration of the free open source openPOWERLINK stack and the additional CODESYS Runtime components from BE.services allow full support of the POWERLINK technology. The configuration of the POWERLINK network is available, fully integrated in CODESYS, with this package.
Anybody heard of it and if possible if it is possible to run on the ctrlX Core ?
The application is controlling frequency inverters on a powerlink network, where it is not possible to change the controller. Therefor the idea is to use our ctrlX core as a gateway between Powerlink and Ethercat, which would be a possibility to run on our EFC inverters.
Best regards
Solved! Go to Solution.
01-13-2023 10:49 AM
Hi
currently it is not planned to support this extension by our ctrlX CORE.
kind regards