03-31-2023 11:47 PM
Hello dear folks,
I would like just to check if any of you has used the CtrlX-Core for Flying-Shear applications and roll-formers (using torque control).
We have a customer that has been using our XM22 for his machines, but now, he wants a better performance but somthing cheaper than XM42.
Is it possible to connect the measuring wheel encoder on the CtrlX-Drive's second port, and then map it as a kind of Encoder-Axis in the CtrlX-Core ? Is it achievable with SoftMotion function blocks? Is there any SoftMotion limitation?
Is it possible to get motion cycle times faster than 2ms?
Is it possible to use Torque/Force Control with the CtrlX-Core and the CtrlX-Drives?
Let me know if we have to stick with MLC for now or we could start testing with CtrlX-Core platforms.
Solved! Go to Solution.
04-03-2023 09:10 AM
Hello
with Softmotion we have no experience here.
But we are currently working for another customer on a solution for flying saw with metal forming.
This project will be with the ctrlX Core, our Motion and the Synchron Motion function.
For more information please contact directly
Hartmann Armin (DC-IA/SDF22)