FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
03-20-2023 04:42 PM
Hello,
I was wondering if there is a limitation on how many axes can I handle with the Softmotion installed in the ctrlX?
As far as I am concerned the Softmotion CNC can handle 4 axes??? So I do not know if the Softmotion has a limitation too,
Many thanks,
Solved! Go to Solution.
03-22-2023 10:46 AM
Hei
The limitation is the export version.
That meas you can interpolated only 4 axis at the same time.
This is the limitation for each kineamtics.
But you can have more than one kinematics
03-22-2023 04:14 PM
Hello FranzClt,
Thank you for your answer but I am refering to how many axes can handle the Standard Softmotion Package, not the Softmotion CNC,
However thanks for the clarification in regard to the 4 axes of the CNC,
03-30-2023 03:55 PM
Hello,
CODESYS Softmaotion does not have any restrictions regarding the number of the axis The limitation is caused by the cpu load of the controller (e.g. our ctrlX CORE). And this depends on the ctrlX CORE hardware (X3/X7/...) itself, the apps running in parallel, is multicore activated and the configured task cycle time.
kind regards
04-03-2023 08:39 AM
Ok, thanks!
06-12-2024 11:13 AM
Hello,
I am using a ctrlX Core X7 with version 2.6, Softmotion 4.15 and ctrlX package 1.20 and it seems that there is a limitation on how many axes the Softmotion can handle...
Has anything changed between the versions?
This is important as I though that there was not a limitation but it seems that there is...
06-14-2024 01:53 PM - last edited on 09-09-2024 09:15 AM by CodeShepherd
Hello
In Version 2.xx CODESYS change the licence model to pay per number of axis.
That means you have to reorder additional axle licenses.