FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
09-20-2022 11:02 AM - last edited on 09-27-2022 08:03 AM by CodeShepherd
I have installed Git with the trail licence in my virtual machine. In here it is working correctly. WORKS version 1.16 & SVN 4.4.0.0.
When i try to install exactly the same package in my Host device ill get the following error?
What might cause this enequility?
09-27-2022 08:04 AM
Moved this question to here from topic "Version Control - SVN or GIT".
11-22-2023 03:27 PM - edited 11-22-2023 03:35 PM
Please install current version 1.20.5 as there were some fixes implemented for the CodeMeter tool that is part of the CODESYS installation in ctrlX PLC Engineering. For older versions you will have to uninstall ctrlX WORKS completely and reinstall it.
You could also add system report from the ctrlX WORKS (see How to generate a system report and switch on additional traces) and also the installation log files that are located under "C:\ProgramData\Rexroth\PackageManager\Logs". Simply zip that folder and provide it. We are working on putting all this files to the system report together.