FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
12-20-2022 12:01 AM
Hello,
I made a small HMI using the visulazaiton tool in CtrlX Works, the same way i used to with Indraworks. The problem is that i can't find a way to enter data into my variable because the Input Configuraiton is missing the "on mouse click" feature in the properties window.
Here is what i looks like for Indraworks:
Solved! Go to Solution.
12-20-2022 07:40 AM
Can you tell us which version of ctrlX PLC engineering and element type you are useing?
Workng on my side:
12-20-2022 08:24 AM
Did you check your Filter settings and the Advanced checkbox in the Properties window?
Here you can define, what properties are displayed.
12-20-2022 10:29 PM
Thank you for the help! This was the issue. Clicking on "Show all catagories" fixed the issue, i now see all of the input configuraions, including the "on mouse click" option.
06-08-2023 02:58 PM
I just ran into this issue too.
Can settings like this please be left alone and stop changing things trying to assume what someone may or may not want!!!