10-05-2023 02:05 PM
Hello,
After enabling softmotion (4.12.0.0 package install) on a ctrlX WORKS V-0120.2 PLC project the message "Could not open library CXA_SoftMotion_BusTaskInterval 4.10.0.0 beacuase it has not been installed to the system" appears. I tried to download from the subsequent dialogue but it failed. Please see attached picture for more info.
Is this library necessary, if so how can I get a copy?
Many thanks
Solved! Go to Solution.
10-05-2023 03:28 PM
The library should already be installed. In the Library Manager, select Placeholders and map the library manually:
10-17-2023 08:34 AM
Hi,
if this version of the library is not available set the placeholder manually to the one, that is available with your installation. Maybe there's a new/other version available.
kind regards