Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

CODESYS WebVisu in ctrlX COREvirtual not reachable

CODESYS WebVisu in ctrlX COREvirtual not reachable

bschmidt
New Contributor

Hello,

I am trying WebVisu on ctrlX CORE virtual 1.20. It is working with the default network settings as shown below. So that is definitely an improvement over earlier versions. But when I change to Port Forwarding mode there is no response from port 8080, even though I can access the ctrlX CORE web UI and PLC at 8443. Do you know what port I should be using in this case?

Best regards,

Brian

bschmidt_2-1684792179225.png

 

bschmidt_1-1684792122470.png

 

 

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

As you see all ports that are forwarded you have to 8080 also to the forwarded ones otherwise no communication data is forwarded to the Windows port and so cannot be received there. For example:

8022:22,8443:443,8740:11740,4840:4840,2069:2069,2070:2070,18080:8080

Here all communication going the ctrlX COREvirtual port 8080 will be available at Windows port 18080.

Please also have a look to the how to "Communicate between a ctrlX COREvirtual and other application"

EDIT: Moved to own topic from this one.

That works, thank you. After adding this to the default forwarding list I can now access webvisu at http://192.168.1.67:18080/webvisu.htm (in my case). I expect it should work from an external device, if I could disable the Firewall on my Bosch PC that is running the virtual CORE. 🙂

Best regards,

Brian

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist