FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
10-05-2022 09:51 PM
Hello,
This is similar to the other post about subscribing to MQTT broker. I am using the Cedalo Mosquitto broker on ctrlX CORE. I can successfully publish and subscribe to it using Node Red. Below are the settings that are working for Node Red. I am trying to make the same settings in Device Bridge, but it never connects. There are two choices: MQTT Connector and MQTT Url Connector. I guess I have to use MQTT Url Connector, because MQTT Connector has no place to enter username and password. (Mosquitto is using secure Tls connection on port 8883 and I must enter in Node Red the same username/password I configured in Mosquitto).
Mosquitto client:
Data being published by Node Red:
Example of failed connector configuration in Device Bridge:
Best regards,
Brian
Solved! Go to Solution.
01-13-2023 11:34 AM
I forwarded your question directly to the Support of the DeviceBridge app. See store area for more information.
04-13-2023 05:57 AM
Hello,
New arm version released having provisions to input username and password
Kindly use credential management to input the credentials and link it to Device / Connector wherever credentials are needed
Note: Unable to attach the snap version due to its size constraint. I will share it via adhoc sharing
Kindly send a sample mail to the below id. shall revert
Email ProductSupport.EIA@in.bosch.com
Thanks
Product Support Team