Hi together, One of our customer is testing now WebIQ to decide if it's convenient for their applications. He has the questions below; 1. How is it possible to specify the color of the image in a Widget Button. (e.g. green enabled, black disabled) 2. How to change the image in a button dynamically with a PLC variable? 3. How to change the displayed color when a button or input widget is locked? 4. Layout: How is it possible to design different layouts? 5. Dialogbox: 5.1 How is it possible to make the Header invisible? 5.2 Can scripts be used to open the dialog and then make different settings depending on a variable? E.g. by type=0, then Text with Value1 and Errofeld(Label) visible by type 1, then Text with Value2 and and Errofeld(Label) visible 6. OPC-UA: How to open an own messagebox dialog when changing the value of an OPC-UA variable "Error"? Or start an action o a value change, or describe local variables? 7. Are there detailed documents explaining what we can do with commands in "scripts" and "CSSs"? Kind Regards, Emrah Emre
... View more