Dear Community User! We are updating our platform to a new system.
Read more: Important information on the platform change.

cancel
Showing results for 
Search instead for 
Did you mean: 
SOLVED

ctrlX core virtual stuck on booting

ctrlX core virtual stuck on booting

Servodude
Established Member

Hello all

 

I am trying to start the virtual core but it is stock on booting in ctrlX works. 

I can see from the terminal window, that the virtual machine is finished booting.

Trying to access the core directly from the browser gives an unknown error.

 

It has previosly worked on my PC but now I am thinking if my PC is overloaded, since the fan is running all the time.

The model, CPU and installed RAM is

 

LEN_ThinkPad_T460

Intel(R) Core(TM) i5-6300U CPU @ 2.40GHz 2.50 GHz

8,00 GB RAM

 

Closing all programs except ctrlx Works and firefox doesnt help.

Any good ideas ?

 

2 REPLIES 2

CodeShepherd
Community Moderator
Community Moderator

The unknown error indicates that there is still some data in your browser cache but no connection to the ctrlX COREvirtual.

Do you have any VPN client or similar active? Because this would prevent your browser and ctrlX WORKS of getting access to control. You could try to run it in port forwarding mode then.

Thank you for providing the solution, it works now using the port forwarding allthough it is still running very slow.

 

 

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist