FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
01-17-2024 01:41 PM
Hello,
I downloaded and installed ctrlXWorks v2.04.
All Engineering softwares are on 2.4.1, but not ctrlXDRIVE Engineering, it's still 1.20.5
Is that right or is something wrong?
Solved! Go to Solution.
01-17-2024 02:58 PM - edited 01-17-2024 04:07 PM
In ctrlX WORKs there is no new version of ctrlX DRIVE Engineering included. As we are using it as a platform and give the possibility to insert other software. Please download the new version and install it into it. Afterwards you can choose which version should be started via the tree dot menu at the name of the tools.
01-18-2024 07:27 AM
additional information
beside the separate installation of the the ctrlX DRIVE engineering (Link to Collaboration room) be aware that the DRIVE engineering version number is not linked to the WORKS version anymore. The last version of the DRIVE Engineering is the 1.26 (date 18.01.2024). The selection of the version you start via Works can be selected by the 3 dots (see screenshot)
01-18-2024 10:59 AM - edited 01-18-2024 11:00 AM
it seems that link to collaboration / file is not working at the moment.
If I understand right, DRIVE is now single and not a part of ctrlXworks anymore. So version of DRIVE doesn't matter? I can still work with 1.20.5 (or a newer one but I don't find any download)
01-19-2024 07:33 AM
Yes.