ctrlX Works crashes in server mode

ctrlX Works crashes in server mode

sebas
New Poster

Hello,

when I start ctrlX Works in server mode and try to run the virtual ctrlX Core, I get the following errors (ctrlX Works App crashes):

sebastianW_0-1727771812948.png

After ctrlX Works reopen, I can see that virtual ctrlX Core is running, I can stop it.

However, when I try to start virtual ctrlX Core again, I get the same errors.

The ctrlX Works version I use is 2.6.1.

Thank you in advance

6 REPLIES 6

CodeShepherd
Community Moderator
Community Moderator

Could you please create a system report in ctrlX WORKS via the questionmark symbol, so we can get some more information?

What do you mean by "server mode"?

 

Sure, System Report is attached. 

By server mode I mean starting ctrlX WORKS with a specific port as param:

sebastianW_0-1727782561845.png

 

CodeShepherd
Community Moderator
Community Moderator

Thanks for the report. Please tell us the command/parameter used.

Using the Windows Command Prompt, I changed the directory to:

C:\Program Files\ctrlX WORKS\ctrlX WORKS\WRK-V-0206\


and executed the following command:

ctrlx-works.exe --port=4242

Then, in the ctrlX WORKS (http://localhost:4242/devices), I simply pressed Start ctrlX COREvirtual and the errors shown at the beggining appeared.

CodeShepherd
Community Moderator
Community Moderator

Just did a quick test on my side with ctrlX WORKS version 2.6.3 and it is working fine. Could you try updating your version and test again?

ctrlX WORKS - server mode runningctrlX WORKS - server mode running

Update:

We faced this problem before but should be solved in ctrlX WORKS version 2.6.3.

ctrlX WORKS update to version 2.6.3 solved the issue 😀

Thank you for your help!

Icon--AD-black-48x48Icon--address-consumer-data-black-48x48Icon--appointment-black-48x48Icon--back-left-black-48x48Icon--calendar-black-48x48Icon--center-alignedIcon--Checkbox-checkIcon--clock-black-48x48Icon--close-black-48x48Icon--compare-black-48x48Icon--confirmation-black-48x48Icon--dealer-details-black-48x48Icon--delete-black-48x48Icon--delivery-black-48x48Icon--down-black-48x48Icon--download-black-48x48Ic-OverlayAlertIcon--externallink-black-48x48Icon-Filledforward-right_adjustedIcon--grid-view-black-48x48IC_gd_Check-Circle170821_Icons_Community170823_Bosch_Icons170823_Bosch_Icons170821_Icons_CommunityIC-logout170821_Icons_Community170825_Bosch_Icons170821_Icons_CommunityIC-shopping-cart2170821_Icons_CommunityIC-upIC_UserIcon--imageIcon--info-i-black-48x48Icon--left-alignedIcon--Less-minimize-black-48x48Icon-FilledIcon--List-Check-grennIcon--List-Check-blackIcon--List-Cross-blackIcon--list-view-mobile-black-48x48Icon--list-view-black-48x48Icon--More-Maximize-black-48x48Icon--my-product-black-48x48Icon--newsletter-black-48x48Icon--payment-black-48x48Icon--print-black-48x48Icon--promotion-black-48x48Icon--registration-black-48x48Icon--Reset-black-48x48Icon--right-alignedshare-circle1Icon--share-black-48x48Icon--shopping-bag-black-48x48Icon-shopping-cartIcon--start-play-black-48x48Icon--store-locator-black-48x48Ic-OverlayAlertIcon--summary-black-48x48tumblrIcon-FilledvineIc-OverlayAlertwhishlist