FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
10-01-2024 10:48 AM
Hello,
when I start ctrlX Works in server mode and try to run the virtual ctrlX Core, I get the following errors (ctrlX Works App crashes):
After ctrlX Works reopen, I can see that virtual ctrlX Core is running, I can stop it.
However, when I try to start virtual ctrlX Core again, I get the same errors.
The ctrlX Works version I use is 2.6.1.
Thank you in advance
Solved! Go to Solution.
10-01-2024 11:09 AM
Could you please create a system report in ctrlX WORKS via the questionmark symbol, so we can get some more information?
What do you mean by "server mode"?
10-01-2024 01:41 PM
10-02-2024 09:49 AM
Thanks for the report. Please tell us the command/parameter used.
10-02-2024 12:07 PM
Using the Windows Command Prompt, I changed the directory to:
C:\Program Files\ctrlX WORKS\ctrlX WORKS\WRK-V-0206\
and executed the following command:
ctrlx-works.exe --port=4242
Then, in the ctrlX WORKS (http://localhost:4242/devices), I simply pressed Start ctrlX COREvirtual and the errors shown at the beggining appeared.
10-02-2024 01:14 PM - edited 10-02-2024 01:21 PM
Just did a quick test on my side with ctrlX WORKS version 2.6.3 and it is working fine. Could you try updating your version and test again?
Update:
We faced this problem before but should be solved in ctrlX WORKS version 2.6.3.
10-02-2024 01:59 PM
ctrlX WORKS update to version 2.6.3 solved the issue 😀
Thank you for your help!