FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We are updating our platform to a new
system.
Read more: Important
information on the platform change.
02-23-2023 05:03 PM
Hello,
is it possible to install ctrlX WORKS via command line ? I mean an automatic installation on some PCs with a command so that the IT-admin has no to much to do with that.
Solved! Go to Solution.
02-27-2023 10:06 AM
Hello st_ctrlX_user,
yes, the setup supports the following parameters:
ctrlx-works-1.18.2.exe /Path="{installFolder}" /Mode={mode} /Silent=yes
Regards,
Oliver