FORUM CTRLX AUTOMATION
ctrlX World Partner Apps for ctrlX AUTOMATION
Dear Community User! We will start the migration process in one hour.
The community will be then in READ ONLY mode.
Read more: Important
information on the platform change.
02-23-2023 05:03 PM
Hello,
is it possible to install ctrlX WORKS via command line ? I mean an automatic installation on some PCs with a command so that the IT-admin has no to much to do with that.
Solved! Go to Solution.
02-27-2023 10:06 AM
Hello st_ctrlX_user,
yes, the setup supports the following parameters:
ctrlx-works-1.18.2.exe /Path="{installFolder}" /Mode={mode} /Silent=yes
Regards,
Oliver