08-25-2023 09:11 AM
ctrlX Works 2.02 is release. I update my ctrlX core X2 from Version 1.20.4 to 2.02.
But In the licenses ,ctrlX CORE License-PLC Standard is not installed
do i need to modify other settings?
Solved! Go to Solution.
08-25-2023 03:32 PM
In the version 1.20 the PLC licenses are different to 2.02 and cannot be used vice versa. So you have to replace yours or at least add the new ones. Following see the new licenses.
PLC licenses |
Material number |
Name |
Basic |
R911421866 |
SWL-XC*-PLC-PLC*XOS******-BANN |
Standard (add-on) |
R911421867 |
SWL-XC*-PLC-PLC*XOS******-NNNN |
Advanced (add-on) |
R911421868 |
SWL-XC*-PLC-PLC*XOS******-ADNN |
Performance (add-on) |
R911421869 |
SWL-XC*-PLC-PLC*XOS******-PRNN |
08-29-2023 10:53 AM
I bought the license of ctrlX CORE License-PLC Standard.
can i update my CtrlX2 to Version 2.02 for free?
11-15-2023 12:25 PM
No, it will cost an update fee. Please get in contact with your known sales person.